Part Number: ADS1259
Hello,
recently I am in a cooperation with an external company.
in which we developed a circuit board that requires 2 ADS1259 for reading sensors from 0....5V over SPI with a maximum frequency of 8MHz,
the processor is a MK20DX256VLH7 Cortex-M4, which is clocked at 96MHz. the Information from both ADS1259 is compared(substracted) and put into a PID to drive a current source for a TEC. so far so good, but I assume that it is too slow based for our TEC.
so let me explain and hope that you can help me solve or guide me in solving the following questions:
what I understand is:
based on the FIFO principle that the both ADS1259 start in, which is continious mode, the 24 bit data is recorded, written to a buffer on the microprocessor. and then the other ads1259 takes over, doing the same as the previous ADS1259. The values are compared in the PID which drives an output MAX5144 DAC 14 bit. the information from both the sensors and max5144 are then read processed and displayed on a small oled screen 10x a second or 100x a second.
what I dont understand is:
1how can I calculate the processing speed of one ADS1259, processing 24 bit as fast as possible. (starttime, collect data, stoptime, senddata to the microprocessor.
is there a PDF or a book, or a Online Seminar that explains this quite well?
I would like to know how to select the right ADC converter for the right application
how do I know that it is fast enough, did I select the right Microprocessor?)
( I really like to understand the magic behind this, so that I can adapt it for other projects)
2 how does the FIFO mode between both ads1259 and the MAX5144(SPI to analog output(0...5V, no further communciation just out) affect the processing speed of the PID control loop (PID_library Arduino from Brett Beauguard)
3 Is there a better PID algorithmn on the market that reacts faster based upon the input signals from the both ads1259?,is there a pdf for this?
4 I would like to know how I can calculate the time one ads1259 needs to process continious 24 bit data start in contnious mode and send data buffer and then stop. how can I adapt this for other ADCS ?
5 how does this account for two ads1259 doing continious mode in FIFO? if the processing of data is done in the following order= 1,2,3 whereby ads1259 =1, ads1259=2,MAX5144 =3 and for;;? is this the best method that exists?
6 is my microprocessor the right one with one SPI Bus?
many thanks, for taking your time to read all this.
and have a nice weekend.