The DAC7811 datasheet refers to the ability to interrupt a command by de-asserting SYNC/ before the 16th falling edge of SCLK. Do I explicitly need to issue a "Daisy-Chain Disable" command before the SYNC Interrupt will work correctly? Is that what is implied by Stand-Alone mode?
7.4.3 SYNC Interrupt (Stand-Alone Mode)
In a normal write sequence, the SYNC line is kept low for at least 16 falling edges of SCLK and the DAC is
updated on the 16th falling edge. However, if SYNC is brought high before the 16th falling edge, this acts as an
interrupt to the write sequence. The shift register is reset and the write sequence is seen as invalid. Neither an
update of the DAC register contents nor a change in the operating mode occurs.
Thanks in advance for any assistance.