Other Parts Discussed in Thread: ADS8860
Hello,
For a low-noise application we are currently looking into the ADS8320.
However, I'm having some questions about the noise spec in the datasheet...
Normally, assuming the SNR is tested with a full-scale sine wave input, there should be a simple relation between the SNR and the noise spec, right?
To calculate the input-referred RMS noise, I would use; 10^(-SNR/20) * Vinrms (and Vinrms = Vpp / (2 * sqrt(2)) for a sine wave)
So that the ADC RMS noise translates to; 10^(-90/20) * (5V/(2*sqrt(2))) = 55.9uV RMS
However, the datasheet specs RMS noise on 20uV RMS?
1) Am I missing something here, or do in interpret hte noise spec wrong?
2) How does the noise/SNR scale with changing the reference voltage (we're using 2.5V)
Thanks in advance!
Best regards,
Sven