Hi,
Is it possible to use the matlab interface with tsw1200 and ADS6422EVM???
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is it possible to use the matlab interface with tsw1200 and ADS6422EVM???
Thank you
Patrick,
I believe you can. There is a .zip file available under Design Notes (one of the 4 tabs the top: Home/Forum/Video&Files/DesignNotes).
Look at ADS64xx FAQ.
Philip
Hi,
As Philip pointed out, yes. But you would need to get the correct folder of code. The original folder of Matlab code that came on the CD with the TSW1200 had only a few devices supported, and more devices were added over time. The original code had a list of devices at runtime that could be selected. At some point it became too cumbersome to have one folder of code to support yet more devices, so we began to make a folder of Matlab code just for each device family. There is a folder of Matlab code that was posted here recently that supports the ADS64xx devices, so you would need to search for that. I only point this out so you don't grab one of the other folders of Matlab code such as from the TSW1200 CD and then wonder why you can't use it for the ADS6422.
Regards,
Richard P.