Is there an IBIS-AMI model available for the ADS42JB69 data converter?
Also need a Power Aware version of the IBIS model. The IBIS model posted on ti.com is for IBIS v4.1. I think it needs to be above v5.0 to include power aware information..
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there an IBIS-AMI model available for the ADS42JB69 data converter?
Also need a Power Aware version of the IBIS model. The IBIS model posted on ti.com is for IBIS v4.1. I think it needs to be above v5.0 to include power aware information..
Hi Jim,
Is the ami model only setup for typ corner? I do see the other 2 corners in the ibis model but that parameter is grayed out in the actual AMI model. Do you have another file that explains all the Tx settings? There is a pdf that accompanied the models but it is not very descriptive. I am looking for some mention of the parameters that the user can toggle and what are the recommended settings and what each of the other levels would do if altered.
Thanks,
Uttara