Part Number: ADS1115
Other Parts Discussed in Thread: TLV2462
Hi,
I need help to properly reduce the differential voltage applied to the ADS1115. My circuit is like in the following picture:
I need to measure differential voltage in order to get positive and negative values.
Since I don't know the signal polarity, I have to add two voltage dividers to be within the maximum ratings for each pin.
The readings from AIN0-AIN1 are correct, the readings between AIN2-AIN3 are not. They are definitely below the expected values with a large variance.
From this post (e2e.ti.com/.../2519803), I understand that the input signal (circuit) and the ADC have to share the ground, but since I have to use two voltage dividers I don't know which is the right way to connect the signal to the ADC.
1) Is my circuit topology correct to properly reduce the differential voltage?
2) How do I have to correct it to get accurate measurements?
3) If I add two zener diodes (MMSZ5226B-7-F - 3.3v) as in the schematic, readings are correct up to about 0.8v, after they are below the expected value. Which is the right way to protect the ADC differential input?
Thank you in advance.
Fab.