Other Parts Discussed in Thread: LMK04828, DAC38J82,
Hello,
I am new to this DAC.
I have dac38j82 and lmk04828. I cannot figure out how to program these ICs even using the GUI provided by TI.
Could anyone provide the register settings relative to my case:
F = [1.5 ... 512]MHz
So Fdac = 1024MHz (minimum acording to Nyquist rule).
M=2
N=16
S=1 (is it Fdac = 1gsps ?, as far as I understand I need 1.024gsps ?)
L = 4
F=1 (bytes per frame)
K=20(frames per multframe)
Lane rate = (M*N*1.25*S*F)/L = 2*16*1.25*1gsps*1/4=10gsps
Is it correct?
SYSREF = Fframe / K.
Is Fframe = Sample clock ?
SYSREF = 1024MHz/20 = 51.2MHz (max)
I would be gratefull if anyone provide register setting so that I could figure out what's going on in the DAC and understand the internal structure.
-Thanks in advance