Part Number: ADS1292RECG-FE
Other Parts Discussed in Thread: ADS1292R, , ADS1292
Hello, I am using the board of ADS1292RECG-FE of your company. I have not developed the board myself. Use the bought ADS1292R circuit board, the computer installs the software, the software is downloaded from the TI website, after installation, the Device ID: ADS1292R; Fireware Version: 1.12; GUI: 1.11; the software installation is completed, and the USB to MINI-USB cable is connected. ADS1292R circuit board and computer, no lead wire, found that the software is collected, the ECG is zero, but the breathing reaches 80 ~ 130 (the photo as below), it is reasonable to say that there is no lead wire, ECG and breathing should not be zero? How to set up the software or what measures can be taken to eliminate respiratory interference? Breathing should be zero when there is no test. There is only the circuit schematic of ADS1292 in ADS1X9XECG-FE User manual. Where can I find the circuit schematic of ADS1292R? The ADS1292R tests ECG and breathing at the same time. Isn't it the 9-core 4-lead lead wire on page 40 of the manual? What kind of lead wire is used, what is the specification of the lead wire? Please reply as soon as possible, thank you very much!