This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

ADS7945: Handling of unused analog input terminals

Genius 5350 points

Replies: 2

Views: 156

Part Number: ADS7945

Hi support team,

I have a question regarding unused analog input terminals of ADS7945.

If the customer doesn't use a pair of analog input terminals (AINxP, AINxN), can he left them open?
Or is it necessary to take measures such as pull-down or pull-up  and so on?

Sincerely,
M. Tachibana

  • Hi Tachibana san

    It is recommended to pull down unused ADC analog inputs to GND to avoid any possible crosstalk.

    Thanks & Regards
    Abhijeet
  • In reply to Abhijeet Godbole:

    Hi Abhijeet-san,

    Thank you for kindly teaching me.
    I understood that unused input terminals should be pulled down..
    By the way, is it okay for pull-down resistors to be 1 kΩ ~ 10 kΩ?
    Or are there any restrictions on the resistance value?

    Sincerely,
    M. Tachibana

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.