Hi TI team,
We are using DAC9881 for generation voltage as per the requirement .
Generate below voltages by setting DAC count 1 time
1. Generated Voltage 1 using DAC - 2.270 approximately
2. Generated Voltage 2 using DAC - 0.317 approximately
Issue Observed:
The DAC output is not consistent. If set the DAC count sometimes i get the expected voltage but sometime i observed lesser voltages.
I attached SPI signal for your reference. To analyze the Data , kindly install the below software from the link
https://www.saleae.com/downloads/
Our Analysis:
If we set the DAC multiple times(10 Times with some delay) frequency of occurence of issue reduces. Means output of DAC is almost expected. Very few times it deviates[Lesser voltage]. But it is not good to set DAC multiple times.
Our expectation --> If we set the DAC one time also, it should provide correct voltage as per the count woithout any deviation
Kindly advice in this situation with high priority.
Thanks and Regards
Manoj