Hello Team,
I faced the problem that High speed data converter Pro could not recognize the TSW14J57EVM.
I have followed the section 4 but I could not make it work.
The driver was visible and installed.
Comparing the jumper setting with a working board I have seen that JP2 was not connected on the working board while on mine the jumper was closing pin 1-2. JP4 on my board was open, while on the working one it was between pin 2-3.
In the used guide is written that JP2 must be open but is a single line in the user guide.
I'm not sure if this jumper came close directly from production, since the card was brand new, same story for JP4.
JP2 and JP4 change some programming modes, but without schematic is difficult to judge the jumper functions.
I think it would help if in section 4 you would add that if PMODEx are not properly set, the driver is seen but board may not be recognized by the GUI.
This may help the troubleshooting.
Beside that challenge, the TSW14J57EVM and the ADC board are now working.
Thanks,
SunSet