Other Parts Discussed in Thread: ADS4142, ADS4125, ADS4145
Hi,
ADS4122 data sheet (SBAS 520 C) page 13
Analog Power ADS4122, ADS4142 (125 MSPS): 112 mW
It is stipulated in.
The ADS4122 and ADS4142 are specified with 65MSPS. (page4 5.Device Family Comparison)
For this reason, I think that the devices written in the 112mW section are ADS4125 and ADS4145.
Is this a mistake?
※ Also Digital Power, LVDS Interface, low LVDS swing section,
Similarly Digital Power, CMOS interface, 8pF external load capacitance, fin = 2.5MHz
Also Standby.
It is also a mistake and I think that it is correctly ADS4125, ADS4145 (125MHz).
best regards
cafain