Other Parts Discussed in Thread: DAC34SH84EVM, TIDA-01187
Hi,
I have one question for my application. I am going to use ADC32RF42EVM to sample RF pulsed signal (352MHz RF and 14Hz period 3.5ms pulse width), the digitized data then is used to process and use the DAC34SH84EVM to create predistorted RF pulsed signal.
For the ADC branch, I am going to use DDC and get the IQ data which forms the envelope signal. Do you know any way to transfer those digitized data over PC host so I am able to plot the data using Matlab (like TSW14J56)? My FPGA platform is based on Kintex-7. I have noticed that there is USB3.0 tranceiver to be integrated on board right? Or I just use USB 2.0 to transfer those data, could it be possible?
Thank you
L.