Other Parts Discussed in Thread: ADS8900B
I have connected to the ADS8900BEVM-PDK board via the PHI controller,I have the installed the relevant GUI from the TI website.
When jumper J2 closed - I havent problem.I can get results with sensor.
But When J2 is open - only the PHI is powered up,the evm board is not powered up and no led glows on EVM board. The board is disconnected both from the sensor connection as well as arbitrarily.
Another jumpers dont change situation.
When J2 closed i have measurements by multimeter in tested point:
DVDD (TP5) -1.75V;
TP6 - 3.3V;
In 5.5V(TP1), 5.2V(TP7), OUT_REF(TP4) - i havent required voltage.
If you look at the layout i can say that problem started after R19(after point "EVM_REG_5V5")
I havent problem with GUI and drivers for GUI because I get results on GUI, problem in disconnect the board.
Could you suggest possible solutions to the problem?
Thank you in advance!