I have a couple of questions on the capture modes of the HSDC Pro. It was not clear in the user guide.
1. If I have averaging enabled with 8 number of captures and the # of samples is set to 65536 and the analysis window set to 8192, does it mean that a total of 65536 * 8 samples is captured and then the first 8192 samples of each of the 65536 blocks is FFTed and then averaged to give the output ?
2. If I have continuous capture enabled with the above setting, is it a rolling average of the last 8 captures or every time the above operation is continued and a new non overlapped average FFT is displayed?
Thanks