This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS54J20: pin compatibility with ADS54J40/60

Part Number: ADS54J20
Other Parts Discussed in Thread: ADS54J60

Hello,

It seems that these devices are quite similar.

1) Can you please confirm they're pin compatible? Drop in compatible?

If not ,what are the differences?

2) I intend to implement DC coupled SE to Diff conversion using LMH3/5/6401 to drive the ADS54J20 . Can I refer to one of the reference designs (eg. http://www.ti.com/tool/TIDA-00823 ), even though it uses ADS54J60/40? In particular the connectivity of Vcm output.

Thanks,

David.

  • Hi David,

    1) Yes, all three devices are pin-to-pin compatible, and are same size (10x10mm).

    2) The reference design you pointed to is ideal for your application. The VCM spec is the same for all three ADS54J20/40/60, so there should be no issue.

    Best Regards,

    Dan