Hello,Dale
Below is the situation of the customer.
>1. Can the customer get the correct out data without any change Control Register (default value)?
Since it is SPI, I think whether data will be needed when clocking out,
At this time, what should be input to SDI?
>2. Keep software mode at the end of Flow 1 until the end of Flow 2, and check the data on the SDO in Flow 2 again.
The result is always 7FFE.
>3. Read the default value of Control Register after power up the device, check if it is 0x000003FF.
Since C17 = READ_EN is in the register,
When reading it, at least C17 needs to be 1
Is it not? In other words, do you think that it will not become 0x000003FF?
Best,regards,
DDdoor