Hi,
I like to know what is the maximum sampling rate when I'm using only one single ended channel e.g. AIN0?
The datasheet says that the max. speed is 30kSPS. Is that the max. speed when I''m using all 8 channels or is it possible to get 30kSPS for one SE-Channel?
At the moment I'm using the following three commands to get my data. SYNC, WAKEUP and RDATA. But after the SYNC command the DRDY goes high for 0,21ms and I have to wait for it to go down.
Is it possible to speed that up?
Hope someone can help and thanks in advance.
Felix