This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] ADC Noise: Is there such a thing as too much gain?

Mastermind 38140 points

Replies: 1

Views: 268

Is there such a thing as too much gain when using precision Delta-Sigma ADCs?

Regards,
Collin Wells
Precision ADC Applications

  • In the seventh series installment, we looked at an example that added multiple external amplifiers to the input of the ADS1261 and measured the resulting noise performance. I then compared these combinations to the ADS1261’s baseline noise performance using its integrated programmable gain amplifier. To make the comparison easier, the noise was plotted at different gain settings for each combination, which offers several insights about how adding external amplifiers to precision ADCs affects performance, as well as how performance changes with gain. Figure 6 depicts the plot.

    Figure 6: Comparing noise performance of different amplifiers plus the ADS1261 as a function of gain

    What are the key takeaways from this example and the plot in Figure 6? Read part 7, “The Effects of Amplifier Noise on Delta-Sigma ADCs,” to learn more.

    Regards,
    Collin Wells
    Precision ADC Applications

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.