Hello,
Could someone say if the DAC121S101QML-SP can have its digital inputs with a dc voltage (3.3V) present without power supply on Va pin?
Is there ESD protections on these pins? If yes, what is the maximum current for ESD diodes?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Could someone say if the DAC121S101QML-SP can have its digital inputs with a dc voltage (3.3V) present without power supply on Va pin?
Is there ESD protections on these pins? If yes, what is the maximum current for ESD diodes?
Thanks
Hello Matthieu,
The DAC121S101QML-SP does have ESD diodes. The max current is 10 mA and the max voltage is Va + 0.3V.
Violating either can impact the life of the part. Restricting the curren to below 10 mA but having the voltage on a pin greater than Va + 0.3V might not cause immediate damage to the part but could impact the life of the part.
Hi Matthieu,
The part has a complex ESD protection circuit. You will not see a diode between the input pins and Va. The diode is a snapback diode and does not turn on until the input voltage goes above 5.5 V.
Hi Kirby,
Thanks for your answer. So I have again two questions :
- In this case, why in the datasheet with cannot have a voltage above Va + 0.3 (and not 5.5V) on digital IO?
- What is the inpact of having digital IO at 3.3V without Va powered. If I'm right in this case ESD diode will not turn ON and the DAC will not be stressed?
Thanks