This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC04: Trouble with 10V operation and 5V clock

Part Number: TLC04

I am using the TLC04 in a single supply operation.  It would appear that I need to use the circuit from Figure 6 of the latest datasheet.  From this figure and the "Terminal Functions" table on page 2 of the datasheet, I have the part connected as follows (schematic pasted at the end of this post):

Pin         Connection

1             +10V

2              350KHz clock, 0 to +5V 

3              +5V: A +10V/2 voltage divider (10K to 10V, 10K to GND, with 0.1uF to GND, same as pictured in datasheet)

4              GND

5              Filter out (AC coupled)

6              pin 3

7              +10V

8              Filter in (AC coupled)

I have successfully used this device with a +/-5V supply, but in the above configuration, it is not passing signals that are in the expected passband (350KHz/50 = 7 KHz, lowpass).

Full disclosure: The +10V input is actually about +10.6V and is heavily filtered with a series 20 ohm resistor, a 1000uF cap to GND , and a 0.1uF cap to GND prior to the TLC04 +10V net.

Am I missing anything?

Thanks!