Part Number: DAC81416EVM
Other Parts Discussed in Thread: DAC81416
Hello,
We have a DAC81416EVM board and I have some questions about how to use it:
1. I have read the Spec of DAC81416(SLASEO0-JULY 2018). There some descriptions about the operation regarding register bits and device pins like:
on page 16, or
on page 18 etc.
The question is: Is the trigger signal determined by the OR-logic of register bit and the device pin? i.e. if the LDAC pin is tied to 0 (active) then the register bit LDAC in TRIGGER Register takes no effect. If I want to use software triggering only, then the LDAC pin must tied to 1 (inactive), is it correct?
2. on page 18 in the spec, the toggle mode is described. What are the differences between toggle mode 0, 1, and 2? According to the spec. only one of them can be set at a time, right?
3. In differential mode (according to the description on page 18), which DAC data register should be written? the positive one or the negative one?
4. There are three type of power-down defined in the spec: device power-down on page 25, internal reference power-down on page 26, and the channel power-down on page 30. What is the difference? Is the device power-down including the rest two? If so, does it means the device power-down has the highest priority?
Thanks in advance!
Best regards,