Hi Team,
I received the following request, can you help me?
#########################################################
I want to ask some questions regarding the AFE ADS1298.
Regarding the detection of Hardware Pace, i tried the approach stated on the design created by Tony Calabria.
http://www.ti.com/lit/ug/slau511/slau511.pdf
http://www.ti.com/tool/tipd111
I used the same design, taking in consideration the modification stated on the design document to remove unwanted noise and frequencies.
Still have problems in the detection of the hardware pace with small amplitudes (Smaller than 4mV with pulses of 100 uS).
We use ECG simulators to produce pace signals, and these equipment are CE certified based on standards IEC 60601-2-25, IEC 60601-2-27, IEC 60601-2-47.
The pace signal produced from the AFE is so small, i know that the Gain is 0.4, but also after setting the gain to 12, the same problem still exists.
Is there any other way to detect the Hardware pace than this analog method?
And also i have another question, Regarding the chip ADS1298R, i only find the 64-LFBGA package, is the 64-TQFP will be available again?
#########################################################
Regards,
Fabio