Other Parts Discussed in Thread: TSW30SH84EVM, LMK04828
I am trying to use LabVIEW to control the DAC34SH84EVM using the FTDI DLL, but there is an error and I can not talk to the device. I am using LabVIEW 2017, hope that is not a issue.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to use LabVIEW to control the DAC34SH84EVM using the FTDI DLL, but there is an error and I can not talk to the device. I am using LabVIEW 2017, hope that is not a issue.
Hi,
Please clarify which EVM you are running. The DAC34Sh84EVM or TSW308x EVM?
Please also advise if you are using 64-bit system. If so, I suspect the error is due to 32-bit dll in 64-bit system. We will need to ask our software team to patch it up.
-Kang
Thank you for the answers. I am trying to load them one by one. For example, I want to change the clock 8&9 divider to 128, which is corresponding to LMK register x04 x0000080, should I configure like the picture shown below? I turned off the GUI and run the LabVIEW code, there is no error but I don't see any change in the output.
Fuquan,
I had posted the information on the 2nd response following your main thread. Please go back to earlier discussion.
There is a forum post that talks about exactly how to interface the TSW308x EVMs through this DLL. Please follow this thread accordingly.