Hi,
I've designed a board with two ADS42LB69. The sampling clock is 125 MHz
and this clock is distributed at two ADS42LB69s.
Now I must synchronize the data acquisition from the four ADCs (2xADC in each
ADS42LB69).
Do you have any suggestions?
In the board I've the possibility to stop the sampling clock and then restart
without glitch.
Is it possible to stop the sampling clock of the ADCs without problems?
Do you think that there is a reduction of the ADC performance?
Is there a maximum time for the stop period of the ADC?
I'm looking forward to hearing from you.
Best Regards