DAC121S101QML-SP: During power-on, I'm seeing a voltage transient on the DAC output. The transient is about 800mV and lasts about 2ms. The DAC supply voltage is ramping up from 0V to +2V during this time (on its way to final voltage of +5V). In the datasheet, it mentions that the DAC output is zero on power up. So, I was not expecting to see any output voltage transient from this part. Is this transient expected during power on when the supply voltage is below +2V?