This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS4246: FPGA interface board

Part Number: ADS4246

We have a requirement to read two analogue input channels from some sensors at 125MSPS or possibly even up to 200MSPS. The proposed design is to use the ADS4246 device with a Zynq FPGA target 

I have suggested that early prototyping of the FPGA IP would be useful in parallel with the hardware design itself.  Are there any evaluation modules that would be suitable to hook up to a Xilinx dev board that would allow us to start developing the IP for the ADS4246 driver?  We currently have some offering a choice of FMC and PMOD connectors.