This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 2
Views: 105
Part Number: ADS5409
Hi Team,
I have a question that I'd like to get your help on regarding the ADS5409.
My customer is wondering if applying a differential signal less than 3.3V to the input pins before its supply voltage rails come up has the potential to damage the device.
I noticed the datasheet defines the max voltage at INA/B_P and INA/B_N to be AVDD33 + 0.5V and a min of -0.5V. This leads me to believe the max differential voltage that can be applied while AVDD33 = 0V would have to be less than or equal to 1V.
Can you please confirm that this is correct?
Thanks,Mitchell
In reply to Vijayendra Varma Siddamsetty: