This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

ADS7883EVM: SPI communication with another board with different GND

Prodigy 50 points

Replies: 1

Views: 109

Part Number: ADS7883EVM

Hi,

I'm trying to read data from the ADS78883 using SPI with an FPGA eval board. I power the ADS7883 with a standard DC supply while the FPGA board receives power from my PC via USB. Is this an issue in terms of ground? How should I connect the boards so that they have the same ground?

Thank you

  • Hello,
    Yes, this is an issue with the grounds. All the grounds should be connected together.
    Does the eval board the FPGA have a ground pin/test point that can be connected to the ADS7883 EVM? One wire connecting the two board grounds should close the loop.
    Regards
    Cynthia

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.