Other Parts Discussed in Thread: SN74LVC3G07
My issues is that sometimes after power up (like 1 in 3 times), I got stuck with nearly the same output value (check below my examples). But this only happens, when the power supply also got powered up at the same time.
I also have a fuse on my PCB and when i remove it and insert it again, I never got this error. For PDWN pin i used the RC circuit, like it is in the data sheet (R = 1k and C = 2.2nF). I have tried also an 33k for R, but it have not changed anything.
I have sometimes read that pulsing the PDWN can help, but I can not test it, cause of the PCB design.
Example of raw output values (in dec) of the channel one and two:
Channel 1: 8388608.0
Channel 2: 8388608.0
Channel 1: 8388608.0
Channel 2: 8388616.0
Channel 1: 8388616.0
Channel 2: 8388610.0
Channel 1: 8388616.0
Channel 2: 8388624.0
Channel 1: 8388623.0
Channel 2: 8388611.0
Channel 1: 8388616.0
Channel 2: 8388615.0
Channel 1: 8388612.0
Channel 2: 8388615.0
Channel 1: 8388612.0
Channel 2: 8388615.0
Channel 1: 8388615.0
Channel 2: 8388735.0
Channel 1: 8388639.0
Channel 2: 8388671.0
Channel 1: 8388624.0
Channel 2: 8388640.0