hello,
could you tell me how to change the input level of J13? I want to input 3.3V level to TRIG_IN.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello,
could you tell me how to change the input level of J13? I want to input 3.3V level to TRIG_IN.
Takuma,
For 3.3V level input signals, on switch SW7, turn on switch 4 and turn off the other three switches.
Switch SW7 controls the voltage used by the FPGA bank that the TRIG signals are connected to. The available voltages are as follows:
SW1 ON, SW2, SW3, SW4 OFF = 1.4V
SW2 ON, SW1, SW3, SW4 OFF = 1.8V (default)
SW3 ON, SW1, SW2, SW4 OFF = 2.5V
SW4 ON, SW1, SW2, SW3 OFF = 3.0V
Only one switch should be ON. Other values can be obtained but the user would need to swap out a resistor. See sheet 31 of the attached schematic. Care must be taken to not create a voltage that is outside the specified allowable values of the FPGA.The FPGA maximum specified input voltage for VCCIO is 3.15V
Regards,
Jim
Hello Jim
thank you. so you cannot use the 3.3V IO into this EVM?
Do i need to set the VCCIO of trigger source below 3.0V, or level shifting?
Ito