Part Number: TSW1400EVM
I am trying to generate a slow phase modulated signal 48M samples in duration (single channel) using the TSW1400EVM with the DAC3482EVM by reading in the samples from a csv file. I understand from the data sheet that the TSW1400EVM supports up to 512M in pattern generator mode - maybe I'm misinterpreting the spec. When I try generating this signal, I do not observe the expected modulation at the output of the DAC3482EVM. However, when I back off the total sample count from 48M to 24M samples, the modulation is observed. I carefully inspected the 48M sample csv file and confirmed that the phase modulation is indeed embedded within those samples so I'm left with the impression that I've run into some sort of memory limitation with the TSW1400EVM.
Should I be able to playback a single-channel signal of duration 48M samples with the TSW1400EVM?
Chris