Part Number: ADS1118
Hi team,
customer use ADS1118 for thermocouple measurement and use temperature integrated in device for compensation of thermocouples.
here is a question is that does is measure ambient temperature or its self temperature?
if it measure itself temperature, it will have error because the device will heats. In customer project, when the start, the IC temperature is 28℃, after it work some minutes, the temperature will up to 34℃.
could you give some information about how to use temperature sensor to compensate the thermocouple accurately?
in the datasheet, it show that the sensor can be used for system-level temperature monitoring or cold-junction compensation for thermocouple. what's the system -level? and how to compensate without being influenced by itself?
thank you