Hello experts
- I am looking for a ADC chip set with 16 bit or 24 bit resolution
- with on chip capture buffer/FIFO of 1024 samples and it must have a interrupt line
- this interrupt line which only interrupt the ELB-REV4 (AM335X based device) once capture buffer is half filled 512 samples and
- then ELB-REV4 (AM335X based device) can read data from the ADC using SPI or any interface
- power consumed by this ADC must be as low as of the order of 2mW even if power consumed is bit high its ok sampling rate can vary from 10 SPS to 1000 SPS
Please suggest any ADC chipset that satisfies the above points