Hello,
could you please let me know the correct value for ADS8555 supply voltages HVDD and HVSS.
If I use the internal VREF (2.5V) with input range of +/- 2*VREF, can I use supply voltages 5V +/- 5%
and -5V +/- 5%, considering tht the real input value range is +-4V?
If I use an external reference, for example 1.5V, with input range of +/- 2*VREF, can I use supply voltages
of +/-3V?
Thanks.
Marco