i have a problem,the VCM of ads4449 is 0.95V,but the datasheet of ads4449 say the voltage of VCM is 1.15V,and after I used the RESET siganl,the output signal of bit[2:0] is 3'b110,the datasheet say the bit[2:0] should be3'd010 after RESET.when I enable the 14 bites output,the bit[2:0] always be 3'b000,the bit[13:3] is right.I really do not know why,I need your help.