Part Number: 430BOOST-ADS1118
Tool/software: Code Composer Studio
Hi,
We are trying to connect a 430BOOST-ADS1118 to a MSP-EXP430G2ET. We have changed the XXX2533 part which is on the MSP430 board with the one supplied in the 430BOOST-ADS1118 kit. Everything is working fine,and we can see the temperature on the screen of the 430BOOST-ADS1118 board.
We have two questions ?
Q1. Is there any way I can get the temperature that I am seeing using my thermocouple on a file. Can I use CCS or any software to tap the 430Boost-MSP-EXP combo stacked dual-boards to get the data on to a file. I am trying to do some measurements which also needs calibration and the temperature is in the high range ( 200 + Degrees Centigrade ) . SO , I am trying to get the data off line so as not to get burnt by the flame.
Q2. Is there any way I can program the "new" Part ( The XXX2533 ) with a higher temperature threshold, the programmer on the CCS is not allowing to me to do so.
I have tried both CCS 5.3 and the latest 9.1 and I am sorry but I am unable to program the part.
Please some advice would be awesome
Thanks
Sudipta Sen