Hi
could you help check below schematic? and give your comments if there are some wrong connections?
I_total_A_P/I_total_A_N is one input
I_total_B_P/I_total_B_N is another input
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
could you help check below schematic? and give your comments if there are some wrong connections?
I_total_A_P/I_total_A_N is one input
I_total_B_P/I_total_B_N is another input
Max,
There's not too much to comment on for this schematic. Generally this is an easy device to configure.
I assume that the inputs are connected to some sensor. If there is any input filtering, that would be something that I would like to look at. Often, we would put some differential and common-mode RC filtering at the input.
For the ALERT/RDY pin, this should be connected to the VDD through a pull-up resistor, similar to the SDA and SCL lines. However, if they are not using this function, pulling it down to ground through a resistor is ok.
It appears that RB84 is a 10 Ohm resistor. I would generally use something smaller like a 1 Ohm resistor. The average current may be only 150uA, but with digital circuits, the instantaneous current is much larger. Because of this, I would use low impedance and no inductive connections to the supply.
Joseph Wu