Other Parts Discussed in Thread: ADS8681, ADS8638EVM-PDK, ADS8638, ADS8568EVM-PDK, ADS8568
HI Staff
Evaluated using the ADS8681EVM-PDK,
Please let me know because there is an unknown point
Q1: When the input is open, 2V can be seen at the input terminal.
Is this not a problem?
Q2: Also, please tell us the basis for this 2V.
* Can you provide an equivalent circuit for the analog input section?
Q3: The signal to the analog input terminal is driven by an external opamp,
A 470ohm Damping Resistor is connected to the output of the opamp.
Is this not a problem?
Q4: When using the USB-GUI software of the ADS8681 EVM-PDK, when the power is first turned on,
All CH-1 measurements were to measure 0 every time.
It went back after repeating the CH setting several times, but some cause
Do you understand?
There is no particular problem after the second power on.
best regards
cafain