Hi support team.
SBAS680 Page-25 Table-1
Table 1. Input Overvoltage Protection Limits When AVDD = 5 V or Offers a Low Impedance of < 30 kΩ
If RS in Figure-68 is less than 30kΩ, does this mean that there is no problem?
Perhaps, I think that 30kΩ is not about RS, but about the impedance of the AVDD line.
If I can, I can see the sentence that you want it to be close to 0Ω.
"The results indicated in Table 1 are based on an assumption that the analog input pins are driven by very low
impedance sources (RS is approximately 0)."
In my circuit, I design with RS of 470Ω.
Moreover, noise reduction is carried out by putting 0.1uF in AIN_nP and AIN_nGND after RS.
If there is a problem with such a circuit, I would like advice.
I am concerned about the last sentence on Page-25 of SBAS680.
"Note that higher source impedance results in gain errors and contributes to overall system noise performance."
How large does "higher source impedance" mean?
SBAU245A Page-39
This circuit uses RS=357Ω and 0.01uF.
Regards,
Dice-K