Part Number: ADS1232
Hello,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1232
Hello,
Hi Uwe,
Welcome to the E2E forum! One possible issue with startup is related to the state of the PDWN pin. We are in the process of updating the ADS1232 datasheet with additional information. The current datasheet discusses the Power-up Sequence and timing with respect to PDWN pin going high. The information is on page 23. There is a requirement that PDWN must be held low for at least 10us after both AVDD and DVDD have reached nominal operating voltage.
It appears that you can control the PDWN based on the schematic. On power-up I would suggest holding this pin low, bring it high, then pulse (minimum of 26us low time) the power-down pin which will reset the device to a valid operating condition. This is the information that will be added along with some suggested timing. It is possible that what you are actually seeing is an issue where the device is improperly starting causing an error in the conversion result. Most of the time this is seen when power is cycled off and back on, but can also occur on initial startup.
Following the PDWN pulse, you should issue the offset calibration. This is accomplished by sending a minimum of 26 SCLKs to the ADS1232.
Here is a suggested startup timing:
Best regards,
Bob B