Other Parts Discussed in Thread: ADS131A04
Hello, This is a question about the analog input signal range which will not trigger an out-of-range error in the status register. According to the datasheet (www.ti.com/.../ads131a02), the permitted analog input voltage range is from AVSS - 1.65 to AVDD + 0.3 Volts (with charge pump enabled). This would indicate that tying either input (AINxN or AINxP) to the ground would not trigger an out-of-range error, but when we try this on the evaluation board, the F_ADCIN error bit and the corresponding bits in STAT_P and STAT_N indicate an overrange/underrange error.
I am unable to find any clear definition of the voltage that triggers this error. The description of COMP_TH (fault detect comparator threshold) seems to indicate that no error should be triggered when the inputs are within 5% to 95% of the input range (when configured to the maximum range). Is there some application note which gives more detailed information about this?
Thanks