This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1013-Q1: Single end

Part Number: ADS1013-Q1

Hi TI-team

My customer want to use the ADS1013-Q1 as a single-ended input.

1. Connect AIN1 to GND.
2.The resolution is 0 V to 2.048 V at voltage level for 12 bits, and 2048 to 4095 for AD value.
   (Half the range of the differential case)
Is this recognition correct?

 

Best Regards,
Koji Hayashi