Hi
I'm trying to set outputs on my DAC60508 connected to a microcontroller but I'm not able to do it. Shutting down outputs by writing the config register works. Changing RefDiv and gain settings also works (I see the output dropping from 2.5V to 1.25V). However, writing on the output register does not change output voltage. I tried both modes synchronous and asynchronous (by setting LDAC bit on trigger register) and nothing. I tried writing DACx register 8 to F and even broadcast messages, but still outputs don't change. I connected a scope on SDI, CK and CS signals and all looked good, even the scope decoded the signal correctly (for example DAC1=0x08FFF0 or 0x080000). I tried different baudrates also although I assume the SPI communication works fine since writing into config and gain register work.
Any ideas? I also tried with another board but the result was the same.