Other Parts Discussed in Thread: CDCE62005, LMK04828BEVM
I was running a setup back in March-April of this year that produced an output frequency of 131.027MHz which is now 138.197MHz running the same setup file.
Below is my setup file...I've verified the correct input clock of 153.6MHz is being applied.
x00 x0880 x01 x0100 x02 x8002 x03 xF001 x04 x4068 x05 x3E60 x06 x2900 x07 x0000 x08 x0000 x09 x8000 x0A x0000 x0B x0000 x0C x0000 x0D x0000 x0E x0000 x0F x0000 x10 x0000 x11 x0000 x12 x0000 x13 x0000 x14 x0000 x15 x0000 x16 x0000 x17 x0000 x18 x0007 x19 x0000 x1A x0020 x1B x0000 x1C x0007 x1D x0054 x1E x0000 x1F x0002 x20 x2400 x22 x1B1B x23 x0000 x24 x0000 x25 x0000 x26 x0000 x27 x0000 x28 x0000 x29 x0000 x2A x0000 x2B x0000 x2C x0000 x2D x0000 x2E x0000 x2F x0000 x30 x0000 x7F x0004 CDCE62005 Registers Freq:153.600000MHz Address Data 00 68040320 01 68800301 02 83800302 03 EB040303 04 68860304 05 11280A55 06 440F3F76 07 3DF8FBC7 08 20009D98