For the ADS8528,…
The datasheet shows +/-5V as a minimum operating voltage for HVDD/HVSS.
What are the impacts running at this minimum level?
I ask since when I review the data sheet, I see the input range is given as +/-2 x Vref, so if Vref = 2.5V, the input range is +/-5V. But, the electrical specification table/device performance is for the condition of HVDD = 15V, HVSS = -15V. I do not see information in data sheet about impact on device performance for the condition when HVDD = 5V and HVSS = -5V.
I understand it may not be able to run to the rails… but what if we guarantee that the channel input voltage will be less than 4.5V max, then what will be performance?