This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

ADS1243: ads1243 DRDY low active, but Sometimes the level is always high, What causes it , Most of the time it's good.

Prodigy 210 points

Replies: 1

Views: 65

Part Number: ADS1243

ads1243   DRDY low active,  but  Sometimes the level is always high, What causes it ,  Most of the time it's good.

  • Hi User5214405,

    It is possible that the PDWN pin does not have a good connection.  This pin must be pulled logic high for the device to convert.  Also, you must have a good clock source either from the crystal or externally derived clocking source.  If this clock source is intermittent or stops, conversion will also stop.

    Best regards,

    Bob B

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.