HI,
I do have customer would like to to use ADS124S08IPBSR into thier project and possible help to review the schematic ?
Meantime ,possible help to advise for the below?
1. All Sensors input are analog Single-End
2. Do we need to "Buffer" the analog signal before coming to ADS124S08?
3. How do we design "Full-Scale" 24-bit with Single-End signal input and uni-polar AVDD?
4. Is there any note for code programming? only by-pass PGA?