This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1293: Common mode amp BW

Part Number: ADS1293


In the attached reference design for the TI ADS1293 found in your app note, it would appear the BW of the common mode amplifier is 16 Hz  (1/(6.28*10 M * 1000 pf). This can't be right. What am I missing? Seems like the BW should be > 180 Hz. 1293 reference design.pdf

  • Hi Brian,

    This is a mistake and you are correct. We are working on getting this revised. Decreasing the size of the resistor to 1Mohm moves the cutoff frequency to 159Hz, which is what it should be. 

  • Hi Alexander,

    Thanks for getting back to me. As an aside, what process would you recommend for optimizing the value of R15 in the reference design - or what value do you recommend for R15 given that the resistor is 1 Mohm?

    Brian

  • Hi Brian,

    I apologize for the delay here.

    R15 is the gain resistor, Rg, so it depends on how much gain of the signal you would like. This can be simulated using the attached file. 

    Upon further inspection of the original circuit, I think using 10Mohm is acceptable. While the cutoff frequency is indeed ~16Hz, (shows 14.96 in the simulation), the gain at 60Hz is still ~47dB, which is sufficient. 

    You can play with the file by changing the values of the resistor, voltage sources, etc, and running an AC simulation by going to Analysis -> AC Analysis -> AC Transfer Characteristic...

    3323.RLD_Loop.TSC