Part Number: DAC80508
Other Parts Discussed in Thread: REF6225
Originally asked in this thread:https://e2e.ti.com/support/data-converters/f/73/t/836424
Moving this question to a new thread
Andrzej asked: "
How to connect external reference voltage to this DAC since its output is as default also configured as output?
In DAC8568 chip the internal reference was disabled by default."
Paul: "we anticipated the case where the user wants to use an external reference. The reference current capability is fairly low (±5mA), so during startup, the internal reference and your external reference will conflict with each other but only with this low current. The DAC will either sink or source current depending on the voltage of the external reference. As long as the abs max table is not being violated, there will not be any damage. This conflicted state will exist until the reference is disabled."
Andrzej: "In regards to the reference. It is very strange and unusual solution to connect output to output.
especially given the fact that external source of reference voltage is unknown
e.g. it may be very strong output of OPA or super precision/delicate/expensive external reference voltage source."